I am looking at using the DRV8824 in a new design. I have experience with the DRV8834 which has a variable decay input based on the resistor value to ground that is placed on its input. The 8824 input is documented as either high (slow decay), low (fast decay) or open (mixed - fast for 75% of PWM cycle). Does the device support the addition of resistance to ground to change the mixed decay to something other than the 75% in a similar fashion to the DRV8834 or is it limited to the only the one mixed type documented in the data sheet? I would like to be able to implement a 50% of PWM cycle with this part if possible.