Hi,
I have an application with a brushless motor with a commutation frequency of around 1400-1500Hz.
On the DRV10983 datasheet, the maximum "electrical frequency" is specified at 1000Hz.
Is this the actual max commutation frequency, or can I expect to reach frequencies of 1400-1500Hz.
For my application, space if vital, and it's important to keep size minimal.
thanks,
Brian