Dear Sir, please answer
1) We'd like to use DRV8432 along with dsPIC30F4012 (Microchip) http://www.microchip.com/wwwproducts/Devices.aspx?dDocName=en010338 We have 6A DC motor Maxon 148867 and we'd like to use Parallel Full Bridge Mode (fig 15). Could you be so kind as to report: have you experience with the use of a DRV8432 with dsPIC30F4012? I need to clarify : are these chips compatible in principle for Parallel Full Bridge Mode?
2) In Parallel Full Bridge Mode (fig 15): half bridge A connected in parallel to half bridge A; half bridge C connected in parallel to half bridge D? So we have like a one bridge of high-power?
TIA
Sincerely
Vladimir Naumenkov
www.agat.by