Hi,
I recently began looking into the DRV8301 for a 60V 70A brushless motor driver. One of the main design goals is to keep the efficiency very high at low output power, so when I first saw the device I figured it would use the buck regulator to reduce gate drive power usage. But that doesn't seem to be the way it's used.
So, two related questions:
1) How efficient is the charge pump regulator used for the gate drive?
2) And, if it doesn't compare well to the buck regulator efficiency, could I set the buck regulator to 12V? 15V? and use it to drive the gates, either directly via the GVDD pin or indirectly through PVDD1 and the charge pump regulator? (The goal with the second option, of course, is to get much better efficiency from the charge pump with a lower PVDD1, so if it doesn't that idea is moot.) Obviously the PVDD1 pin will be fine at 12 or 15 volts instead of 60, but is there a problem with the boost voltage going up to 70 volts or so if PVDD1 is at 12V? And, if the charge pump regulator is backdriven at 15 volts, will it shut down politely and let the external regulator take over, or complain a lot?
One more secondary question - is my battery voltage too high to use safely with the DRV8301 and its buck regulator? Fully charged, the battery voltage could reach 62V. It sounds like I would at least need to put in more anti-surge protection, compared to a gate driver rated for 100V or more, but I am not sure which measures would be most appropriate.
Thanks!