HI,
Can any one tell which parameters effect the commutation frequency?the motor which comes with DRV10983 EVM speed around 360Hz,and in datasheet max it is up to 1kHz ,so how can i increase the frequency more than 360Hz?
i searched for the datasheet of the motor which comes with EVM but i didn't get pl provide me the link to the datasheet of the motor (ZWL12-22-2.5I)?
Thank you