Hi,
We are using a DRV8432 to drive 2 DC motors. It works succesfully but with this limitation: after powering the board (being it unpowered for several minutes) the driver detects a fault condition (Fault pin low) and the only way to get the motors spinning is by touching (with a naked finger) some ground point. Once they are working, touching gnd isn't needed anymore.
This is the setup:
- PVVD=GVVD = 12V
- PWM frequency: 20kHz
- Bootstrap capacitors: 100nF
- OC_ADJ resistor: 22k (the lowest value specificed in the datasheet)
- 220nH inductor in series with each motor
The motors are relatively low current, and the driver doesn't heat a bit when running.
Any help will be very much appreciated.
Martín.