Hello,
I am concidering using the DRV8823 in a product which I am designing to drive 4 DC motors.
It seems that the DRV8823 has everything that we are looking for (12V input, current sense speed control, Full H-bridges, SPI enabled to save pins).
However, the product is required to brake when the motors are not being driven. This of course means shorting the motor pins (both sides GND or both sides VCC).
Q1. Does the DRV8823 do such a thing? or will we require external logic / relays to achieve this?
Another question (actually a confirmation) software related,
I would like to pulse SSTB to latch (like the latch in a shift register) the data as an extra security measure but it looks like pulling it low will disable the outputs (according to the data sheet).
Q2. If I want continouous operation, will I be forced to keep SSTB high and just accept that the first 16 bits will be auto latched?
Thank you in advance.