Hello all
I am designing a stepper motor kit for students using DRV8825. I powered up the trainer kit with 12V, 2A, the datasheet says that the operating current should be 8mA maximum, but i don't think giving 2A would cause any issues since the chip should draw the current it needs. The reason I am pondering over this point is the fact that whenever i connect my stepper with the kit the chip (DRV8825) starts heating up.
I am using a Vref of 1.65V and Rsense of 0.2 ohms. What do you think might be the cause of the chip heating up?