Hi
DRV11873 4 Questions.
1) It's written on Figure1 and 3 of page7 of data seat (SLWS237A) with "100% Duty".
Can PWM input be input to Duty 100% ?
2) It's revolving to 20000rpm by Duty 100% in Figure7 of page8 of data seat.
How many volts is VCC ? (2.7V? or 3.3V? or others)
3) Page8 of Figure8 is revolving to 25000rpm by VCC=16V.
How many percent is Duty? (50%? or 100% or others)
4) It's revolving even at most 25000rpm by a chart of Figure8.
Please tell the condition to make them revolve to 25000rpm.
(The specifications of the motor and loads, etc.)
Best regards