Team,
Can you check what phase is startup phase of DRV11873?
W or V or U? or It depends on other factor like motor location?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Chloe,
I tested start-up in the EVM. Based on this, in starting Phase V goes high 100%, phase U goes low and phase W remains open so V and U are start-up phase not W.
Start-up does not depend on rotor magnet location.
I hope this answer your query.
Best Regards
Milan