I have few doubts about DRV10983:-
1)How I will get maximum speed(In my application it has to get a minimum speed of 1500 rpm but i stucked at 750rpm) of Runtian motor on maximum load? Can any suggest me to change any default settings of motor that might helpful to me.
2)I connected another bldc of mine to DRV10983 for a fan application what's the problem I'm facing is that I'm not reaching the maximum speed(I'm getting 800rpm only,It doesn't reach its maximum ratings also,while I measured I get V-12,I-0.85) on load.So,Can anyone suggest to overcome this and my motor specifications are given below:-
The specifications of bldc are:
Operating voltage-24,Current-2.1(Max.),RPM-2000(on load),Pole-10,Phase resistance -0.7.