This is for Mr. Milan Rajane.
I have used the EVM and am not able to write on to EEPROM. Upon clicking of eeWrite message displayed is " make sure power supply is higher than 22V" even though it is 24 V.
Few minutes back motor stopped rotating even though with the parameters filled in, it was rotating at 260 RPM with load, as desired, for few hours. It is powered by 24 V battery. Can you please advise as to what may be going wrong?
I have not reported that I lost a 10983, with current limit of 2A