Hello, I have built my own circuit using the DRV8840. The schematic is below. I believe that the 9V supply is in spec (greater than 8.2V) and my logic level of 5V is still ok according to the data sheet. I've checked the solder connections and the wirings several times, so I believe there must be something wrong with my design. When I power up the device, and I set ENABLE to 5V, nothing happens. The voltage levels are all what they should be, but the motor doesn't actuate.
Note that I'm not using a PWM, I'm driving with DC 5V.
Any ideas on what the issue might be? Thanks!
Matt