Here are just several brief notes/descriptions of the laboratory setup:
- There are tree pendulums, each driven (balanced) by its own DC motor (motor supply voltage is 6V, max. current 1 A). The three F28377D Delfino Experimenter Kit microcontrollers (one per motor) control the pendulums in real-time. Between the microcontrollers and the motors are motor drivers. The goal is to control pendulums positions of very fast oscillatory dynamics of spring-connected inverted pendulums.
Question about motor drivers:
Using external (coming from microcontrollers) PWM input signals to Low-Voltage H-Bridge Driver DRV8832, is this driver appropriate for 4-quadrant DC motor MOTION control?
Note: I prefer DRV8832 it versus DRV8837 due to current limiter and current sensing.