I took the BoostXL board and spun the kit motor from the DRV8301-LS31. I then removed the MOSFETs and replaced with wires to my inverter using the same Vishay MOSFETs as the DRV8301-LS1. Motor spun.
Finally, I connected the modified BoostXL board to my custom inverter using IR MOSFETs that require gate driver current of 0.656A (=105nC/160ns). Motor does not spin and I get a fail.
Is the default max gate current from the DRV8301 set at the max setting? Is that peak or average?
I used wires from the board to the inverter but placed a large cap at the inverter. Will the wire length effect the circuit?
Thanks Alan