Dear TI Team,
We are using DRV3201 for BLDC motor control and prepared a HW board same as the application note SLVU846A–January 2013–Revised July 2013.
- No error on the ERR pin.
- We observe , Highside PWMs are shifted from zero and we cannot understand the reason. LOW side pins shows PWM output.
- We use the same values of 22microH, 10microF and a fast response schottky diode on SW and pin 29.
- We have not connected MOSFETS. If we connect MOSFETS, we do not see any PWM waveforms.
- what is the typical waveforms seen on pin 29, 30 and voltage levels? Please share.
Any help available for the above points?
Best Regards
Girish Karpur
Bangalore