Dear Sir ,
I have just started to use the TI make DRV8825EVM and connected to the stepper motor. Using the application program i was able to connect (communicate) and then i configured the settings as per the datasheet (enable=0 , sleep & reset=1 , chopping current =0.5amp) connected the VM to 12Vdc and then when i command from the window to step the motor. no response and no current is drawn from the power supply. And also one of the observation is the status LED on the board is blinking.
Kindly respond as early as possible.
Thanks