Hi ,
The resistance between GVDD and GND is about only 12Ω.when I connect 12v power to GVDD, the power can be reduced to 0. and then everything cannot work. Why? My board is bad?
Thanks!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi ,
The resistance between GVDD and GND is about only 12Ω.when I connect 12v power to GVDD, the power can be reduced to 0. and then everything cannot work. Why? My board is bad?
Thanks!
Hi,
I am using the DRV8432EVM. It is a new board. I was testing it this afternoon. And the board has worked for 1-2 hours. I found: the out A/B/C/D are not square wave when the outs are disconnected with any other things. Output have big fluctuations when PWM is high/low level. Why the turning on and stabilazing time is not so short as the datasheet says?
Then I turned off and stopped the testing for a while. When I went back and turned on the power, to find that the board cannot work and the 3.3v light is not bright. When I connect 12v power to GVDD, the power can be reduced to 0. and then everything cannot work. I measured the resistance between GVDD and GND, and it is about only 12Ω.Why? My board is bad? But it is a new borad.
I do not know what to do now.
Many thanks!
Best,
Xinjing
Thank you so much, Rick.
The board may be damaged. I tested another board and it can work. But I still can see big fluctuations of the outputs:
When I disconnect its outputs with anything , I can see many fluctuations. Please see Figure1.
When I connect its outputs with a coil (resistance=11Ω), I can see many fluctuations. Please see Figure1.
When I connect its outputs with a 200Ω resistor, the number of fluctuations can be reduced to one. Please see Figure2.
When I connect its outputs with a 100Ω resistor, the fluctuations disappear. Please see Figure3
Why the turning on and stabilazing time is not so short as the datasheet says?
figure1
figure2
figure3
Thanks!
Best,
Xinjing