Hi
Could you tell me how to enter standby mode DRV10866?
Is it that Input PWM is low? If this is correct, How long should the input signal be made Low?
Thanks
Shimizu
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi
Could you tell me how to enter standby mode DRV10866?
Is it that Input PWM is low? If this is correct, How long should the input signal be made Low?
Thanks
Shimizu
Hi Rick
Thank you for your support.
I'm sorry to ask you a question many times.
>An example is a board with a digital input (no duty cycle).
>This will produce 100% motor speed or standby.
Does "no duty cycle" mean "100% On Duty"?
And Is the cause of the following event (red circle) standby mode by being over speed? or over current?
Thanks
Shimizu