Hi,
I have an application, where the motor has to turn at low speed sometimes.
In this special case we are talking of speeds of around 1000RPM. Voltage is around 12V, current for motor about 10mA, Motor has 4 poles.
On some of my PCBs (abt. 10-20% of the 1st pre series production), the motor will suddenly stop at the low speed (around 1000RPM, 4 pole motor).
If I exchange motor with the components from a working device, the problem is still there, so I am sure, the problem comes from the driver chip.
Also the not-running motor works on another driver PCB.
In another posting in this forum I have read, that the DRV10983 is analyzing coil current to determine commutation time. So the question is, if there is some kind of minimum current? Or are there any other things to do to optimize motor operation under low speed/low current conditions?
Thanks for any hint,
best regards,
Martin