Dear all,
Could you answer following two questions?
■Question 1; Are there some concern to use following value of resistor to set Vgain?
I want to set Vgain to x30. You recommend R21=R22=30kΩ, R11=R12=1kΩ at Figure 15.
However I want to use E6 line resistor.
So I think that R21=R22=33kΩ、R11=R12=1kΩ or R21=R22=47kΩ、R11=R12=1.5kΩ.
I am able to think that changing of Vgain, but are there some other concern?
And which is the value recommended?
■Question 2; Are there some trade-off to use 0.1uF capacitor for C2?
You recommend 10nF for C2 at Figure 15.
However I think to use 0.1uF to get more stability.
Are there some trade-off things to increase capacitance?
Best regards,