Hello!
Assuming that 0.1uF/35V is a recommended capacitor for pins CP1 and CP2 (CP flying capacitor) on DRV8308, what would be the maximum tolerable capacitance? Or in other words, would the IC remain undamaged if the capacitance is for example 0.22uF or 0.33uF?
Similarly, if the CP storage capacitance (between VM and pin VCP) is changed from recommended1uF to 2.2uF or 3.3F, would that have an adverse effect on the IC?
Many thanks in advance.