Hello -
I am building custom hardware, and have a question regarding the DRV8305. On the BOOSTXL-DRV8305, the "PWRGD" and "WAKE" pins are broken out. On the TIDA-00643 reference design, I see that the "PWRGD" pin is pulled logic HIGH (3.3v), and not connected to the MCU. Can I do something like this with the "WAKE" pin as well, or is it recommended to have this connected to the MCU??
I definitely want to be able to set the FETs into high-impedance, so I am definitely connecting the "ENGATE" to the MCU, but based on the data sheet it doesn't seem like the "WAKE" pin is required.
Please advise. Any help is appreciated.
-asifjahmed