Hello,
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
I believe this question will be better served if I move it to the Motor drivers forum.
Hi,
You would need to implement some sort of speed sensor on the brushed dc motor and then close the loop with some sort of controller that would regulate voltage in response to speed.
Sensors include hall sensors, encoders, resolves, etc.
Sorry, read that as brushed DC motor, not brushless DC.
For a brushless DC motor there are drivers that can be used for speed control.
The DRV10866 is an example. It outputs an FG signal from the back-emf of the motor that can be used by an external controller to setup a speed control loop.
Ty for the response,
I was planing on using a DC PC fan with 3 wires, measuring the RPM with the tacho output , puting in a pid control loop and then controlling the speed trought a mosfet.
I'm interested do you have a chip that would hold the fan at a stable rpm, with as little as possible fluctuation. Or something that would hold the fan at a set rpm programmed by either a chip (i'm using an arm development board for now) or some other way.