I am driving a TEC with the DRV593 Evaluation module. This TEC draws 0.9A at 5V when driven directly via a PSU. But through the DRV593EVM I am getting a max of 0.45A. The voltage across the TEC is driven to maximum achieve 5V across it. Does anybody know why this is happening. My input drive level is at 0V (max drive) therefore I would expect full current through the TEC (except small losses in the FET and filter)? Is there some sort of limiting going on? I know that the evaluation module is capable of up-to 3A.