Hello,
I currently have the DRV10983EVM and am using it to evaluate a BLDC motor connected to an 8 blade fan. the fan is used as an optical chopper and for the most part the DRV10983 works fine, my question was with regards to accurate control of RPM speed. We use a photo-transistor to monitor the speed of the blade and I noticed using PWM control there's a minimum delta between my ability to control the speed of the motor, i.e. i have about a 4 hz step in blade speed and i'd like to reduce that down to at least 2 hz. I was hoping to be able to write software to use a micro-controller to vary the Duty Cycle to achieve that resolution but i wanted to confirm that something like this was possible with DRV10983 or would something like the DRV8307 be more suitable for this application (i do have the option to switching to a motor with hall effect sensors). Would the DRV10983 be able to respond to fast changes on its input speed pin?
Thank you for your time