i was trying to follow the motorware lab2c - 3a on a low inductance motor. After a few runs the fault led06 came up as soon as i hit the run button. i read some posts on the possible failure of the driver. but i was using just a small battery pack of 15V on a small motor with very low inductance (measured inductance between phases is 4uh). i wonder what kind of operation may have killed the chip other than overvoltage? i believe the kit is well protected from over current.
thanks
gz