Can DRV8305 be used to control a DC motor?
Using the 6-PWM mode of the Driver IC can the gate of 1 half bridge be set to low and then use the other two half bridges to control a DC motor. Would this idea work?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Jyotirmaya,
Yes, the DRV8305 can be used as described.
We have many other devices that are specifically designed to drive a DC motor, such as the DRV8701 with external FETs or the DRV8871 with internal FETs. See the links below: