iam using drv8301.Iam facing a little problem with buck converter that without load my buck converter output is 5V but after connecting the microcontroller the output drop to 3V.
please help
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Shashank,
The resistor values chosen are correct for 5V output. Please look at section 9.2.2 of the TPS54160 datasheet to confirm the inductor and output capacitor selections are correct.
If they are, please post a screen capture of the voltages before and after the inductor. Also, you can post questions regarding the regulator on the Non isolated DC/DC forum