Hi,
I would like to know which is the lowest speed we can get with DRV8308.
Until now, we have designed a PCB based on this driver and configure to run in a closs-loop mode and it works fine from 13Hz (200rpm) to 233Hz (3500rpm)
But when I try to run on lower speed, It doesn´t work properly.
I don´t know if there is any speed limitation or I have to check spi parameters again.
Thanks in advanve.
Igor