Other Parts Discussed in Thread: DRV8312, CONTROLSUITE
Hi,
I have a BLDC motor project and i use 2 bldc motor this project. Both the some. I want to drive 250 W bldc motor with hall effect sensor.
It must be;
Vs = 24 or 36 V
Is(max) = 8 or 10 A
So i discovered TI DRV8332. But i didn't see the hall effect sensor connection when i looked the drv8332 schematic. Do i encode in CPU side the hall effect sensör ? or Is there any ic like this ?
Summary
* I don't want to use mosfet
* I want to encode hall effect sensor wtih anything
* I need more ampere :) (approximately 10 A)
Thank you for repply
Best regards.