Hi whomever it concerns!
Regarding the FaultZ pin.
In application it is pulled up to 3.3V with 100k
In application I have pulled the SDZ low.
Attached the behaviour of the Faultz pin at 4A on the device.
It is not compltely clear to me how to calculate the pull-up at other supply voltage than the 26V. You refer to 26V in the datasheet.
I expected a distinct on/off when a failure due to overcurrent or to high temperature on the device.
Could you please advice?