Hello;
We are designing a motor controller for a motor with a rated current of 0,9A stall current of 8A.
The motor has to be used at stall for a few seconds
I'm looking at the Drv8850. which can be used at 5A continuous @25 degrees
How long can the Drv8850 be loaded with the 8A peak current @50 degrees
We're going to use a fr4 2s2p PCB.
Can anyone recommend better suited controller?
Regards;
Pieter