Other Parts Discussed in Thread: TPS54160
Hello team,
I am supporting an application using the DRV8301 and when EN_BUCK is left floating the device does not power up unless there is an external pull-up, the datasheet recommends to "float to enable".
1. Is there any conditions under leaving EN_BUCK floating is contraindicated and a pull-up is required?
2. What is Absolute Max voltage on EN_BUCK/Pin 55? (Note: I see VLOGIC has a maximum of 7 V, but EN_BUCK is not listed under there).