Hi team,
I have 4 questions below from the datasheet Table 5. Error Conditions and Protective Actions.
The purpose of the question is for a failure analysis.
1. Does ERR pin internally pulled up to VDDIO?
2. Regarding to the "Shoot through protection violated", Is ERR pin pulled low if one of 3 pairs of PWM inputs fails(=both P/N inputs High) or all 3 pairs of inputs need to be fail before ERR pulled low?
What is the failure threshold of ERR pin?
3. There are 5 temperature sensors. Where are they located? Is ERR pin pulled low if any one of 5 sensors detect over temperature?
3-2. If temperature exceed the 2nd threshold and the device enters global reset, how is the ERR pin status? Hi-Z?
4. Regarding to the LOC, what is the power supply for the internal OSC(10MHz)? Is it VCC3? How about the GND?
regards,