Hi,
I need information about Ipeak tolerances which is made by choose of Rpeak resistor. According the data sheet on page 6 in Electrical char. Current controller internal settings says that if I ground the PEAK then the variation of Ipeak is 270mA to 330mA with nominal 300mA. Whats happen if I use a Rpeak instead? Is variation dependent of Rpeak (1%) or should I get 10% variation of Ipeak independent of Rpeak? What is tolerance I can expect over temperature range?
Best regards Boris Ivanic