I am concerned about not being recognized because there is no answer,
I set up the same thread.
(I'm OK that you submit an answer only either thread.)
-------------------------------------------------------------------------------------------------------------------------------------------------
HI, team.
We are looking for similar products of DRV110.
(If it does not exist in the product, it is ok with that.)
I'm understanding that the DMIN (Minimum PWM duty cycle) of the DRV 110 is 7.5%.
So, please tell me about similar products of DRV110 that correspond to one of the following descriptions.
· Products corresponding to duty of 7.5% or less
· When duty is less than 7.5% Skip PWM output (do not output) Product
Could you help me?
Best regards,
Masumi Sekiguchi