Other Parts Discussed in Thread: DRV8305, MOTORWARE
Hello,
I Originally got my motor running using Proj_lab02b but for a number of reasons I had to reinstall everything. Now I am trying to get back to where I left off.
I am able to have the motor spin while the code is identifying the motor, but after calibration the software does not change the gMotorVars.Flag_enableSys from 1 to 0. I have tried changing the parameters in the user.h file, including increasing the USER_MOTOR_RES_EST_CURRENT and IND_EST_CURRENT to 3 and -3. And also tried increasing the USER_MOTOR_FLUX_EST_FREQ_Hz from 20 up to 80 Hz. Even when the gMotorVars.Flag_enableSys does get changed to 0 after identification when I change it back to 1 the motor does not ramp up to the set point of 0.100 krpm.
Here are the identification numbers
Rs=0.078
Lsd_H=Lsq_H=.0004156 but varies wildly from .0022 to 0.0
Flux = .032
The motor I am using is actually an alternator which I am exciting the field to create essentially a permanent magnet motor. it has 12 poles (2 pole pars) My measured stator inductance is .088mH. Maximum current 30A, running at a bus of 15 V right now. on a DRV8305 Boostxl. Motorware.17, CCS 7.0. I also tried running proj_lab02c for low inductance but this did not work either.
Very strange that the system can spin the motor (ramping up to 1000 rpm) during identification and then does not run in normal mode.
Any help is much appreciated.