Hello,
Our customer use the DRV8884.
The customer apply voltage to Decay pin.
Perhaps, there are three threshold voltage at Decay pin.
Vth1: between Vi1 and Vi2
Vth2: between Vi2 and Vi3
Vth3 between Vi3 and Vi4
Could you tell me the value of threshold voltage?
I know it operates correctly by input 100mV, 300mV, 1V, 2.9V.
The customer want to know the tolerance.
one more question
When the customer use Slow/Slow decay, is it possible to left open the Decay pin?
Best Regards,
Naoki Aoyama