Hi,
I'm using a motor that has a PWM range of 0-16v. I have a Pololu DRV8801 driver that is triggered by a WeMos micro controller. Though the prototype is working, and the Vbb = 16v, the max voltage available voltage to the motor during the PWM operation seems to be only 5~6v.
a. Is this normal?
b. If so, are there driver boards that will deliver the entire Vbb to the motor?
Thanks