Hi,
The current input to the motor is measured as 60mA, but the design value is 75mA. What could have caused this change?
Please see the details..
1. RREF = 562K
2. TRQ = 1
3. DECAY = tied to DVDD (slow decay)
4. We use both 1/4 and 1/2 stepping modes in our design and two PWM frequency - 400Hz and 800Hz.
5. Motor current waveform is shown below.