Hello,
Regarding to internal current control PWM frequency on DRV8825, my customer is asking some question.
They are understanding as following.
The step frequency is used to control the indexer logic. The indexer can be advanced at a 250kHz rate.
The current control PWM frequency is used to regulate the current on the output. It is up to 30kHz.
(Question)
If the step frequency(indexer) is used on 250kHz rate, how behaver will current control get?
Can current control (30 kHz) support to indexer with 250 kHz rate?
Regards,
Tao2199