Hi
I want to confirm the function of overcurrent protection and current limit.
According to the description of CS pin from datasheet, the following sentence is said.
But it is not clear for me.
"The voltage across the resistor compares with the voltage converted from the bottom MOSFETs' current.
If MOSFETs' current is high, the part goes into the overcurrent protection mode by turning off the top PWM MOSFET and keeping the bottom MOSFET on"
1.
What is the across voltage that is explained in "The voltage across the resistor compares with the voltage converted from the bottom MOSFETs' current."?
couIs it the voltage at CS pin?
2.
If the bottom MOSFET's current is higher than a current value set as Ilimit = 6600/Rcs, the device goes to overcurrent protection mode.
If overcurrent protection mode is worked once, what is happen to the device?
Is the output current limited by Ilimit value, and output current keep to flow as Ilimit?
Or it keeps low level output?
BestRegards