Hello Team,
I am working with a customer who is looking for a control solution for his project. This is a motor controller/ braking unit. This can be up to 24V and 320Amps. and would like to be able to adjustable voltage.
The system will act similar to a BLDC. In this setup the customer will be using Eddy current braking units, so with those they are aiming to vary the voltage which will linearly vary the current to the coils. If they can adjust the voltage from 1-24VDC with high current capability, that should work.
Do we have any device that can handle the high current that they will see ?
Thank you for you time.
Regards,
Kishen