Hi,
I am using DRV8323H in one our project along with ATMEGA2560 for a BLDC motor Driver.
I am using the DRV8323 in 6 PWM, and proving PWM from Atmega2560 after reading the HALL SENSOR position for the motor.
The PWM frequency is set at 31KHz, and this is very well within the limit of the DRV8323. The current sens resistors of 0.001Ohm are connected on the ckt as suggested. and the gain is set to 40. IDrive is connected to GND with a 75K resistor. and VDS is connected to DVDD with 18K resistor.
I am increasing the PWM gradually from ATMEGA2560 till 40% of PWM the motor runs without any issue, after 40% of the PWM on time, the Driver is entering the Error mode. as i am using the Hardware version for this project i have no clue why this error is being occurred.
Presently the mosfet which is used is with the Gate supply of 4.5V. and the VM is 12V. Does this make any difference? I mean is the error is because of this?
Kindly let me know if there is any why to find out what the error is?
Looking forward for your feedback.
Best Regards,
Shivaraja,N