This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV8432: OC-ADJ calculation

Part Number: DRV8432

Hi All,

Could you please help to provide OC-ADJ calculator information to us??

My customer need to set OC = 2A. Please kindly help. thanks.

  • Hi Pao Wu,

    Please use a 143 kOhm resistor for 2A. The values are approximately linear between each point.

    Please note there is device to device variation to consider. From the datasheet:
    Assuming a fixed resistance on the OC_ADJ pin across multiple devices, a 20% device-to-device variation in OC threshold measurements is possible. Therefore, this feature is designed for system protection and not for precise current control.