My question is around the interface to the microcontroller with using DRV8835. If I pull the MODE pin high can I control the speed and direction effectively with just 3 signals from the microcontroller? AENABLE and BENABLE lines would be PWM outputs. Can A and B Phase signals be tied together to set direction with a single pin?