Hi! We're using the DRV8811 in a 3-axis device and I have a few basic questions about designing in the DRV8811...
- What kind of filtering is typically used / advised on the AOUT and BOUT pins on the DRV8811 device in order to reduce EMI problems? The datasheet makes no mention of this but common sense seems like something would be advisable. We would like to defensively put this in now just to reduce the chance of problems later on down the road.
- What value would be advised for a bulk capacitor on the power supply (VMA / VMB pins)? Obviously it will depend on the motor current; what is the typical advice here?
- Is it advisable / necessary to put overvoltage protection on the power supply (VMA / VMB) to suppress overvoltage transients above the supply voltage?
- We did not get a hold of the DRV8811EVM due to availability problems; unfortunately TI did not post the schematic for this EVM on the web site so the only reference we found to use was this one: http://www.avayanelectronics.com/AE-MDL-STPR1_Schematic.pdf . Are there any obvious shortcomings / problems with that design? (Or better, can I get a copy of the schematic from the EVM, e.g. via e-mail so I have the proven TI reference design?)
- Drive current for our application is going to be 1.27 amps; supply of 24 volts. Our device will be operated in a typical air-conditioned office environment and no other significant sources of heat apart from the three DRV8811 chips will be present on the application circuit board. Thermally, can we expect to be ok using synchronous rectification, a 4-layer board with 2 oz outer layers, 1 oz inner layers and ground planes on all 4 layers with the required thermal vias - or is that pushing the limits?
Thanks in advance for any help!