Other Parts Discussed in Thread: DRV8825, DRV8824, DRV8811, DRV8880, DRV8818
Hello,
Regarding to slow decay mode on DRV8833, my customer is asking some question.
They have confirmed that the motor current is unstable and exceed setting current on slow decay.
(Please refer attached file.)
At first they tried on first decay and mix decay but it happened howling sound on these mode.
At slow decay mode only, it didn’t happened howling sound. So they have been using on slow decay mode.
(Question)
(1) Could you please tell us the possible cause of this behavior(unstable motor current)?
(2) If there is some solution for this behavior, could you please give comment or advice ?
(3) Is it possible to adjust PWM frequency of current control by external?
Or it is adjusted automatically internal?
Regards,
Tao2199