Hi
DRV8320H is used in 1 x pwm mode and three hall sensors are used.
Is it possible to control the direction of spin (clockwise and counter-clockwise) by hardware control pin?
BestRegards
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi na na78,
The INHC input controls direction in 1x PWM mode. Please refer to section 8.3.1.1.3 of the datasheet for details:
The INHC input controls the direction through the 6-step commutation table which is used to change the direction
of the motor when Hall effect sensors are directly controlling the state of the INLA, INHB, and INLB inputs. Tie
the INHC pin low if this feature is not required.